Onze merken

Welkom op de website van Schneider Electric

Welkom op onze website.
		
Hoe kunnen wij u vandaag helpen?
What is the cable entry size or cable gland size on Altivars ATV650, ATV950?
Sizes of ATV650, ATV950 drives
S-A1 : 0.75kW to 5.5kW
S-A2 : 7.5kW to 11kW
S-A3 : 15kW to 22kW
S-B : 30kW to 45kW
S-C : 55kW to 75kW

Products size Gland CAP
ATV650   A1 1x ISO20
2x ISO25
ATV650   A2 1x ISO20
2x ISO25
ATV650   A3 1x ISO20
1x ISO32
1x ISO40
ATV650   B   1x ISO20
2x ISO40
ATV650   C   1x ISO20
2x ISO63
ATV950   A1 1x ISO20
2x ISO25
ATV950   A2 1x ISO20
2x ISO25
ATV950   A3 1x ISO20
1x ISO32
1x ISO40
ATV950   B 1x ISO20
2x ISO40
ATV950   C   1x ISO20
2x ISO63