Onze merken

Welkom op de website van Schneider Electric

Welkom op onze website.
		
Hoe kunnen wij u vandaag helpen?
How do I program the ATV61 analog output for an 0-10Vdc feedback?
Issue:
Program the ATV61 analog output for an 0-10Vdc feedback .

Product Line:
ATV61 / ATV71

Environment:
All serial numbers

Cause:
Need feedback signal

Resolution:
Main menu > Drive > Input / output menu > Set AO1 type to "IOU". Set UOL1  to 0 and UOH1 to 10.