Onze merken

Welkom op de website van Schneider Electric

Welkom op onze website.
		
Hoe kunnen wij u vandaag helpen?
Is M340 SD card compatible with M580?
Question:
Is M340 SD card compatible with M580?

Answer:
No, the M340 and M580 SD card are not compatible. They both have special formatting required by the PLC.
The BMXRMS004GPF memory card is formatted specifically for the M580 CPUs.
NOTE:
If you insert an incompatible SD memory card in the CPU:

l The CPU remains in NO_CONF state.
l The CPU BACKUP LED turns ON.
l The memory card access LED remains OFF.