Hoe kunnen wij u vandaag helpen?

ATV630: what are the minimum parameters that need to be programmed prior to running the motor?

Issue:
What are the basic parameters on an ATV630?

Product Line:
Altivar Process ATV630

Environment:
All

Cause:
Programming

Resolution:
You want to program the parameters in the Main Menu >  Simply Start to protect the motor.