Onze merken

Welkom op de website van Schneider Electric

Welkom op onze website.
		
Hoe kunnen wij u vandaag helpen?
Is there a measured drawing available that shows where AR4601 is installed onto a NetShelter CX2?
Issue:
A customer needs a measured drawing showing the AR4601 installed onto a NetShelter CX2.

Product Line:
NetShelter CX2

Environment:
All models, all serial numbers.

Cause:
A customer wants to pre drill holes in the floor for the AR4601.

Resolution:
See attached file

Schneider Electric Belgium

bijlage(n)
AR4601 Bolt Down Kit Floor Orientation on NetShelter CX2.pdf [69.85 KB]