Onze merken

Welkom op de website van Schneider Electric

Welkom op onze website.
		
Hoe kunnen wij u vandaag helpen?
Can the integrated display on a PM5000 series be replaced?

Issue

User would like to know if the integrated display of the PM5000 series meter can be replaced in the event of damage.

Product Line
PM5000
PM5500

Environment
Hardware
Front Panel Display

Resolution
The integrated display in PM5000 series cannot be replaced. If the integrated display is damaged or found to be defective, the entire meter will need to be sent back for repair.

The only meters with the remote display option can have just the display replaced. Please follow FA344599 for instructions