Onze merken

Welkom op de website van Schneider Electric

Welkom op onze website.
		
Hoe kunnen wij u vandaag helpen?
When will the ATV71 become obsolete?
Issue:
ATV71 obsolescence date.

Product Line:
Altivar 71

Environment:
All

Cause:
Date of obsolescence

Resolution:
The ATV71 480V models will become obsolete on January 1, 2020. There is no update yet (as of Jan 1, 2019) on when the other models will be obsoleted.
See attached official letter from the Product Manager.

Schneider Electric Belgium

bijlage(n)
ATV71 Obsolescence Date.pdf [1.56 MB]