What can cause an InF4 or internal error 4 on the ATV630 and ATV930 Process drives?
InF4 or internal error 4 on the ATV630 and ATV930
Product Line:
ATV630, ATV930, ATV660, ATV960
Environment:
All
Cause:
Read fault access to Indus zone Eeprom (EEPROM APP & EEPROM MC) or EEPROM fault access.
Resolution:
• Factory reset (RAZI: 256 Factotry setting / 512 First power up)
• Replace the control block.