Onze merken

Welkom op de website van Schneider Electric

Welkom op onze website.
		
Hoe kunnen wij u vandaag helpen?
Is it possible to use Ethernet IP and Ethernet TCP on the same network using an ATV630?
Issue:
Usage of Ethernet IP option and the integrated Ethernet TCP on the same network with an ATV630

Product Line:
Altivar 630

Environment:
All serial numbers

Cause:
I have several ATV630 monitoring Ethernet, some have option Ethernet cards and some do not.

Resolution
Ethernet IP and Ethernet TCP cannot be used on the same network.