Onze merken

Welkom op de website van Schneider Electric

Welkom op onze website.
		
Hoe kunnen wij u vandaag helpen?
What causes an INF1 [Internal Error 1] fault on an ATV340 series drive and how do I correct it?
Issue:
INF1 [Internal Error 1] fault on ATV340 series drive.

Product Line:
ATV340

Environment:
All

Cause:
Configuration

Resolution:
The power board rating is not valid.  Check the Identification Menu for the drive's power rating to see if it matches the nameplate.  Cycle power to clear the fault.  If the fault returns contact your local Schneider Electric representative.