{}

Onze merken

Impact-Company-Logo-English Black-01-177x54

Welkom op de website van Schneider Electric

Welkom op onze website.
Populaire vragen (FAQ's) zoeken
What are the Current inputs characteristics of EM6438H meter ?
Current Inputs:

CT primary      :  1 A to 32767 A, programmable
CT secondary :  1 A or 5 A
Operating current range with accuracy   :    10 mA to 6 A
Measured Amps with full range              :     5 mA to 10 A
Suppression current (to disregard negligible load)  :   5 mA to 99 mA
Permanent overload (withstand)   :      Continuous 10 A, 10 s/hr 50 A, 1 s/hr 500 A
Impedance           :   0.3 mΩ
Frequency range  :    50 / 60 Hz ± 2 Hz
VA burden            :     ≤ 0.1 VA at 5 A, 50 Hz

Schneider Electric Belgium

Ontdek meer
Productfamilie
Mogelijk nuttige artikelen
Ontdek meer
Productfamilie