Onze merken

Welkom op de website van Schneider Electric

Welkom op onze website.
		
Hoe kunnen wij u vandaag helpen?
Where can I find the PME 2020 Configuration Manager Tool?
Product Line
Power Monitoring Expert 2020

Environment
Migrations

Resolution
*The use of this component, and any component in the Toolkit, has the potential to modify system configuration and should only be used by competent personnel. Backups of database and/or System Configurations should always be made prior to utilizing tools. Schneider Electric bears no responsibility for changes made as a result of the use of this tool. The component is posted on an as-is basis.*


In order to download the Standalone CM Tool, please login into the EcoXpert website and then select the link below:

Configuration Management Tool v2020

Note:The CM Tool inside the PME_2020 .iso file is only for In-Place upgrade and should not be copied off to use as a Standalone CM Tool. Only the downloaded version is recommended as a Standalone CM Tool.