Onze merken

Welkom op de website van Schneider Electric

Welkom op onze website.
		
Hoe kunnen wij u vandaag helpen?
Is Bacnet option available for Altivar 320?
Issue:
Is Bacnet option available for Altivar 320?

Product Line:
Altivar 320

Environment:
All serial numbers for Altivar 320

Cause:
N/A

Resolution:
No, Bacnet option is not available for Altivar 320.

The following optional communication modules are available:
  • Modbus TCP and EtherNet/IP (VW3A3616)
  • PROFIBUS DP V1 (VW3A3607)
  • DeviceNet (VW3A3609)
  • EtherCAT (VW3A3601)
  • POWERLINK (VW3A3619)
  • ProfiNet (VW3A3627)