Onze merken

Welkom op de website van Schneider Electric

Welkom op onze website.
		
Hoe kunnen wij u vandaag helpen?
Where to find EDS file for PM5560 meter?
Issue
EDS file is required to configure PM5560 meter to communicate over Ethernet/IP CIP protocol. From where it is possible to get this file?

Product Environment
PM5560 with Ethernet/IP CIP protocol

Resolution
EDS file is available along with the f/w release package. It is possible to download the latest f/w installation package from the below-mentioned website.

https://www.se.com/ww/en/download/