Onze merken

Welkom op de website van Schneider Electric

Welkom op onze website.
		
Hoe kunnen wij u vandaag helpen?
How to mount an optional interface card to the Harmony P6 Box?
Goals and Symptoms
As an option of Harmony P6, you can install a cartridge interface (RS-232/422/485, WiFi/Bluetooth) to this product. You can install two slots on the Advanced Box, and one slot on the Standard Box. Some optional interfaces require more than just inserting to the product. For more information, check the pages for each optional interface and User Manual.
The goal of this resolution is to explain how to attach an optional interface to the Box Module.
Causes and Fixes
Here is the video to show How to mount an optional interface card to the Box module