Hoe kunnen wij u vandaag helpen?

What is the difference between D3 and D voltage code for the low consumption D-Line contactors?

Issue:
Difference between D3 and D low consumption D-Line contactors

Product Line:
IEC Contactors and Starters

Environment:
TeSys™ D Contactors

Resolution:
Both coils are rated the same DC voltage.  D3 incidcates the coil provides integral transient suppression.