How can you read the digital input assignments over ethernet on the ATV61/71 Drives?
Issue:
Is it possible to read the digital Input assignment over ethernet for all inputs?
Product Line:
Altivar 61 Altivar 71 and Altivar Process Drive
Environment:
All
Cause:
Communications Inquiry
Resolution:
Yes, you can read Logic/Digital Input Assignments over the network.
See document attached for explanation.
Gepubliceerd voor: Schneider Electric Belgium