Hoe kunnen wij u vandaag helpen?

What operating system is supported by the EcoStruxure Automation Device Maintenance V2.1 software?

Issue:
Operating supported by the EcoStruxure Automation Device Maintenance tool


Product Line:
EcoStruxure Automation Device Maintenance, EcoStruxure Control Expert


Resolution:
The Automation Device Maintenance V2.1 software requires one of the following operating systems:
  • Microsoft Windows 10 32-bit / 64-bit (Professional Edition)
  • Microsoft Windows Server 2016
  • Microsoft Windows Server 2019