Hoe kunnen wij u vandaag helpen?

How do I check if Bluetooth is activated for commissioning EVlink Pro AC with eSetup?

First, ensure that the Bluetooth is activated on your smartphone or tablet.
Check if your EVlink Pro AC is listed on eSetup. If not, it means the Bluetooth is not activated on EVlink Pro AC. In that case you need to:

1- Until there is no Admin badge recorded in the charging station, you can activate the Bluetooth by powering the charging station Off and then On, and wait for the strip light to turn green. The bluetooth will be activated    for commissioning and the session will close after 2 Hours of inactivity.

2-Tap the admin badge on the RFID reader. The Bluetooth of the EVlink Pro AC will be activated and will be closed after for 10 minutes of inactivity.