Hoe kunnen wij u vandaag helpen?

Can I use one external modem for several EVlink Pro AC chargers ?

Yes, connect the modem on the Ethernet network and configure it.
From the factory the modem or gateway is set to 192.168.0.254.
You can change the gateway address thanks to eSetup.