Hoe kunnen wij u vandaag helpen?

How do I move all inputs bits of a 16 point discrete input module to a memory word in EcoStruxure Control Expert?

Issue:
Moving all inputs bits of a 16 point discrete input module to a memory word in EcoStruxure Control Expert


Product Line:
EcoStruxure Control Expert


Resolution:
First, ensure that the "Directly represented array variables" and "Allow dynamic arrays" options are selected in the project settings under variables.
image

To move all 16 input bits of a discrete module, you would use the MOVE_AREBOOL_INT function block. on the input pin enter the topological address followed by the array length :16

image2