How to use the HMI BSC Network Configurator ?
This article is applicable for HMI BSC boxrunning on Yocto Linux (example: HMIBSCEA53D1L0T)
OS: Yocto Linux SE build V1.00.012 or higher (SV: 3.0 or higher)
The BSC Network Configurator is a Web Interface to remotely configure the network interfaces of an HMI BSC box.
The BSC Network Configurator resolves two pain points:
- The need to connect keyboard and screen to the box to configure it
- The complexity of configuring the network interfaces by modifying Linux configuration file
Please find the document attached.