Hoe kunnen wij u vandaag helpen?

Viewing diagnostics of the M580 from the web page

Issue
Where to find information about the M340 from the web page.

Product line
M580

Environment
Internet Explorer/Microsoft Edge, Windows 10

Resolution
Once you have logged into the M580 web page, you will see the M580 Summary which includes Service Status, Network Information, CPU Summary, and Version Information.
M580 Web page
Additional information about the M580 can be found in the Diagnostics tab.
Diagnostics tab on the M580 web page
Additional info