Hoe kunnen wij u vandaag helpen?

Where can you find the ILF fault code number for the ATV320 Drive with an VW3A3616 Ethernet option card?

Issue:

Where can you find the ILF fault code number for the ATV320 Drive with an VW3A3616 Ethernet option card?

Product Line:

ATV320+VW3A3616 Option card

Environment:

All

Cause:

Need to ID which subcode is showing for the ILF fault.

Resolution:

Using the VW3A1101 HMI or the VW3A1111.

-Drives Menu

-Monitoring 1.2

-Diagnostics

-More Fault Info

Internal link fault: code number.

Example sub code 18= EEPROM detected error

ILF fault