Ecostruxure Automation Expert [22.0]: How to set M580 controller to automatically Run after deployment
By default, the M580 Controller will be in STOP mode after successful project deployment and User needs to manually RUN the Controller by giving another Command.
However, User can set the Controller to automatically RUN after Deployment. This can be done by setting the below shown Device configuration settings in Logical devices tab.