Hoe kunnen wij u vandaag helpen?

Can the analog output module METSEPM89M0024 of a PowerLogic ION8000 meter be set via the web server ?

No, the PM8000 analog I/O module METSEPM89M0024 must be installed on the PM8000 energy meter and you can set up the ports using the ION Setup app.


You can find the ION Setup app online and download it from the Utilities and Firmware section