PrismaSeT S - In the reference LVSSD824, would it be possible to mount reference INS 28909 in the duct? Which accessories are needed ?
For PrismaSet S enclosures with lateral duct (including ref.LVSSD824) there is no accessory to mount Switch-Disconnector INS (including ref.28909) inside the lateral duct.
However, it could be done, by mounting on a plate or a DIN rail fixed on the metallic uprights which are at the back of the lateral duct.
Preferably at the top side, due to higher lateral duct front face cover, but the measurements and all the adaptations have to be made by the customer.
However, this size of INS lines up with the modular devices. So it would be possible to install it in the enclosure, on one of the modular rails.
Gepubliceerd voor: Schneider Electric Belgium