Hoe kunnen wij u vandaag helpen?

Is a PBPQOU4A100CEGL630 compatible with part number PBPQOU4A100CEGL630T

Issue:

Checking compatibility

Product Line:

Busway

Environment:

PBPQOU4A100CEGL630

Cause:

N/A

Resolution:

Both part numbers are the same with the exception of the T suffix, which is just the addition of a carry handle option.