Hoe kunnen wij u vandaag helpen?

Ports used by PCT server Client application


PCT1 doesn't use TCP port 2512.


Here are listed ports used by PCT1, the customer can block all others ports to be on the safe side.
• TCP on port 4444 (fixed)
• HTTP on port 80 (default)
• HTTPS on port 443 (default)
• Default server port is port 9091
• Engineering port 32768-61000