Hoe kunnen wij u vandaag helpen?

Can the BMXNOR0200H module's Ethernet communication be reset using IO_DDT (ETH_RESET)?

1. Issue
Some customers have reported that the online help in Control Expert suggests BMXNOR0200H supports Ethernet communication reset via IO_DDT (ETH_RESET). However, this functionality is not supported. The only available method to reset the Ethernet communication is through the module’s web interface.

2. Product Line

  • Module: BMXNOR0200H

  • Software: Control Expert

3. Environment

  • Operating System: Windows 10 / Windows 11

  • Software: Control Expert

  • Browser: Any standard browser used to access the module’s web interface

4. Resolution
After consultation with R&D, it has been confirmed that BMXNOR0200H does not support Ethernet reset via IO_DDT. The only supported method is through the web interface of the module.

Note:
No updates to the user manual are planned. It is recommended to use the BMENOR2200H (Advanced RTU module) instead, which supports Ethernet reset via Device DDT.