Working Offline on configuration files for the SAGE RTUs products
Title:
Working Offline on configuration files for the SAGE RTUs products
Issue:
Users need to build or modify RTU configuration files for the SAGE RTUs but do not have access to a physical SAGE device.
Product:
SAGE 2x00
SAGE 3030x
SAGE 4400
SAGE 14x0
Environment:
Configuration of RTU files without a connected SAGE device (offline scenario).
Cause:
The standard configuration process requires a live connection to a SAGE RTU to create or modify files. When spare SAGE RTUs are unavailable, this becomes a limitation.
Resolution:
SAGE RTU provides a licensed software tool called SAGE Offline Configurator Tool that allows users to work on RTU files without being connected to a physical device.
- The tool can be purchased through authorized distributors or a sales representative.
- Two licensing options are available:
- S2000-OLC-001A0 – Single seat license
- S2000-OLU-001A0 – Unlimited license