Hoe kunnen wij u vandaag helpen?

Why do I get an error when configuring port mirroring across certain ports on an MCSESM203F4LG0 switch?

Question
Why do I get an error when configuring port mirroring across certain ports on an MCSESM203F4LG0 switch, and how can I enable mirroring?

Answer:

  1. Issue

    Configuring port mirroring on MCSESM203F4LG0 fails with error message: "TX mirroring across unit boundaries is not supported"
  2. Product Line

    • Hardware: MCSESM203F4LG0
    • Software Version (SV): 8.7.10
  3. Resolution

    Port mirroring on this model is limited to a single switching chip. Mirroring across the two internal chips is not supported—this is a hardware limitation.

    The MCSESM203F4LG0 has two internal switching chips:

    • Chip 1: Ports 1/1 to 1/12
    • Chip 2: Ports 1/13 to 1/20

    To resolve:

    • Ensure that the mirror destination (primary/monitor port) and all mirror source ports (TX/RX) are on the same chip.
      • Example: Choose the monitor port from 1/1–1/12 and only select mirror sources within 1/1–1/12; do not include ports from the other chip.
  4. FAQ Applicable Conditions

    • This FAQ remains valid unless a new hardware revision explicitly adds cross-chip mirror support.