Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What does the suffix "GRA" designate in a busway plug-in unit, for example, PQ3603GRA?
Issue:
Selection

Product Line:
Busway

Environment:
UL 857, CSA C22.2 No. 27-1973, NFPA 70 Art. 368

Cause:
In most circumstances it is necessary to fully understand the features of a busway plug-in unit which are designated by the suffix(es) added to the standard published catalog number.

Resolution:
The ``G``designates the ground provision, which is now a standard feature on busway plug-in units (and is removable if necessary).  The ``R`` designates factory installed Class R fuse rejection clips.  The ``A`` suffix designates special lugs, most often a copper compression lug, unless otherwise specified by the customer.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings