Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Does Square D offer general duty, heavy duty, or double throw safety switches for use in corrosive environments?
Issue:
Product Design Features

Product Line:
Heavy Duty Safety Switches

Resolution:
Square D general duty, heavy duty, and double throw safety switches are available in different NEMA rated enclosures. See below the different NEMA ratings for each line of switches.
1) GDSS are ONLY available in NEMA type 1 and 3R. They are NOT available in any other NEMA Type.
2) HDSS are available in NEMA types 1, 3R, 4, 4X, 5, 12K,12, 7, and 9 for certain ampere ratings. The NEMA 4, 4X, and 5 are available in 304 stainless steel, 316 stainless steel, fiberglass reinforced polyester, and krydon for certain ampere ranges.
3) DTSS are available in NEMA Type 1, 3R, 4, 4X, 5, and 12 for certain ampere ratings. The NEMA 4, 4X, and 5 are available in 304 stainless steel for certain ampere ratings.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings