Issue:
UL Listed Contactors
Product Line:
Contactors and Starters
Environment:
8911 Definite Purpose Starters
Resolution:
The 8911DPSO starters can be UL listed by using a form U1. It is UR as standard. Form U1 may be obsolete for most of the 8911 starters. The LC1D contactor and LRD overload relays are the possible option that are UL Listed.
UL Listed Contactors
Product Line:
Contactors and Starters
Environment:
8911 Definite Purpose Starters
Resolution:
The 8911DPSO starters can be UL listed by using a form U1. It is UR as standard. Form U1 may be obsolete for most of the 8911 starters. The LC1D contactor and LRD overload relays are the possible option that are UL Listed.
Released for: Schneider Electric Canada