Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the Terminal Lug Data for ALL of the 800A, US and Canada, Heavy Duty Safety Switches (for example, H367, H367R or H367AWK)?
Issue:
Product Design Features

Product Line:
Heavy Duty Safety Switch

Cause:
Terminal lug data

Resolution:
ALL the 800amp Heavy Duty Safety Switches will accept (3) #3/0 AWG - 750 kcmil aluminum or copper conductors per phase.  The Lug conductor(or wire) temperature rating is 75 degree C.

The only alternate lugs are the H8LKE2 compression lug kit, but the compression lugs do NOT allow for any additional or larger wires. See FA120693 for more information on this compression lug kit

More on Safety Switches here.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings