Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Can an elasped time meter be added in the field in a NEMA 3R enclosed contactor or starter?
Issue:
Identify the accessories that can be added to an enclosed contactor

Product Line:
Class 8502/8536 Contactors and Starters

Environment:
Square D NEMA Contactors and Starters

Resolution:
The elapsed time meters for NEMA 3R enclosures are internally mounted and use a special mounting bracket. They can not be installed in the field. Use form G107 when ordering the device for a factory installed elapsed time meter.

Schneider Electric Canada

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings