Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Is a motor operator available for a Class 1 Division 2 HVL/cc. ? What is the price adder for HVL/cc Stainless Steel Enclosure?
Issue:
Motor operator and Stainless Steel Enclosure for HVL/cc

Product Line:
HVL/cc Switchboards

Environment:
Product Features

Resolution:

For Class 1 Division 2 applications, there cannot be any electrical controls or motor operators. Controls such as this, could cause a spark and cause an internal explosion.
There is a stand alone single N3R stainless steel HVL.cc and List price adder will need to quoted thru SE Sales.

Schneider Electric Canada

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings