Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Is HVL/cc available as Duplex? Is there a mechanical interlock for HVL/cc?
Issue:
Duplex HVL/cc and Interlock

Product Line:
Medium Voltage Switchboards

Environment:
Product Characteristics


Resolution:
Yes, HVL/cc has duplex configurations.

A mechanical interlock of the push buttons on the mechanisms is available.

This is available only for HVL/cc with the SEM Mechanism and the switches must be adjacent to each other.


Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings