Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Will a 4-pole TeSys LC1D09 amp through 38 amp contactor mate up with a 3-pole LRD overload relay?
Issue:
3-pole LRD overload relay for a 4 pole LC1D09 amp through 38 amp contactor

Product Line:

IEC Contactors and Starters

Environment:
IEC TeSys D Contactors and Overloads

Cause:
Overload for a 4 pole LC1D09 through 38 contactors

Resolution:
No it will not. The 4-pole contactor`s load connections are spaced closer together than the 3 pole. The overload relay will have to be separately mounted.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings