Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Does Square D offer a QO or Homeline load center for use in hazardous locations (NEMA 7 or NEMA 9 enclosures)?
Issue:
Product design

Product Line:
Load Centers

Resolution:
No, Square D does not offer QO or Homeline load centers for use in hazardous locations (NEMA 7 or 9 enclosures). Load centers are ONLY available in NEMA type 1 or 3R enclosures.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings