Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Can 9001KT or 9001SKT push-to-test pilot light be ordered without a light module?
Issue:
Clarifying if a 9001KT or 9001SKT push to test pilot light can be ordered without a light module

Product Line:
9001K Heavy Duty Pilot Lights 30mm Push Button

Environment:
30mm Illuminated Operators

Cause:
Wanting to replace the housing for the push to test, and not the light module.

Resolution:
Yes. The operator only is a 9001K2L for the K line and a 9001SK2L for the SK line.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings