Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the Horsepower Rating of 8501K Relays?
Issue:
Information on the rated power for Class 8501 Type K relays

Product Line:
General Purpose Relays

Environment:
Class 8501 Type K relays

Resolution:
The 8501KP, 8501KU, 8501KF, and 8501KL relays have the following horsepower rating:
1/3 HP at 120V
1/2 HP at 240V

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings