Issue:
Can the Glass lens/cap for Type K Pilot light be use on Type SK Pilot light?
Product Line:
Push Buttons and Operator Interface
Environment:
Class 9001 Type K/SK Pilot lights
Cause:
Customer need Type 9001SK pilot light with Glass lens or cap. Would like to know if he can use the Glass cap for Type 9001K pilot light
Answer:
It is not recommended for Type SK pilot lights and those with integral metal ring
Can the Glass lens/cap for Type K Pilot light be use on Type SK Pilot light?
Product Line:
Push Buttons and Operator Interface
Environment:
Class 9001 Type K/SK Pilot lights
Cause:
Customer need Type 9001SK pilot light with Glass lens or cap. Would like to know if he can use the Glass cap for Type 9001K pilot light
Answer:
It is not recommended for Type SK pilot lights and those with integral metal ring
| Plastic Fresnel | Plastic Domed | Glass | |
| Amber | 9001A31 | 9001A9 | 9001A6 |
| Blue | 9001L31 | 9001L9 | 9001L6 |
| Clear | 9001C31 | 9001C9 | 9001C6 |
| Green | 9001G31 | 9001G9 | 9001G6 |
| Red | 9001R31 | 9001R9 | 9001R6 |
| White | 9001W31 | 9001W9 | 9001W6 |
| Yellow | 9001Y31 | 9001Y31 | 9001Y6 |
Released for: Schneider Electric Canada