Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the Standard Cartridge Contact Rating of the 8501XO Relays?
Issue:
Electrical rating information for the cartridge used on the 8501XO relays

Product Line:
Relays and Timers

Environment:
NEMA 8501 Power Relays

Resolution:
Inductive 35% Power Factor : 120VAC NEMA Rating A600, Make 60amps 7200VA, Break 6amps 720VA, Continuous Amperes 10A,
Resistive 75% Power Factor: Make, Break and Continuous 10 Amperes

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings