Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What are the replacement mounting screws for an LA or LH type breaker?
Issue:
Mounting Hardware for unit mount LA or LH type Circuit Breakers

Product Line:
Molded Case Circuit Breaker

Resolution:
The mounting screws are part number 4812514450 for a bag of 4 screws, 12 - 24 x 3.25" long.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings