Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Are auxiliary contacts available for the LP1/LP2K K-Line contactors?
Issue:
What is the part number for the auxiliary contact used with LP1/LP2K Contactors?

Product Line:
TeSys™ K Contactors and Overload Relays

Environment:
Contactors and Overload Relays

Resolution:
Yes, the standard LA1KN auxiliary contacts can be used on the DC controlled contactors. However the four pole units will not work on the LP4 and LP5 low consumption DC controlled devices.

Schneider Electric Canada

Explore more
Range:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Range:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Center
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings