Issue:
What is the part number for the available auxiliary contactors on Tesys K Contactors?
Product Line:
IEC Contactors and Starters
Environment:
TeSys K contactors and accessories
Cause:
Would like auxiliary contact for the TeSys K contactors
Resolution:
Yes, standard LA1KN** screw clamp or LA1KN*** slip-on connector type auxiliary contacts can be used .
What is the part number for the available auxiliary contactors on Tesys K Contactors?
Product Line:
IEC Contactors and Starters
Environment:
TeSys K contactors and accessories
Cause:
Would like auxiliary contact for the TeSys K contactors
Resolution:
Yes, standard LA1KN** screw clamp or LA1KN*** slip-on connector type auxiliary contacts can be used .
Released for: Schneider Electric Canada