Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the part number for the mechanical interlock, starter and reversing contactor for the Class 8736 Type SDO2?
Issue:
Mechanical interlock for reversing NEMA starter or contactor

Product Line:
NEMA Contactors and Starters

Environment:
8736 Type S Starters

Resolution:
Mechanical Interlock = 9999SM6
Starter = 8536SDO1V__, complete V__ with required control voltage code.
Reversing contactor = 8502SDO2V__, complete V__ with required control voltage code.

Note: This applies to Class 8736 Type SDG2, SDW11, SDT43, SDR3 and SDA1 enclosed reversing starters as well as they use the 8736

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings