Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Can 9013 FSG pressure switches be used on air compressor applications.
Question:
9013 FSG pressure switches application assistance

Issue:
9013 FSG Pressure Switches can be used as air compressor.

Product Line:
Pressure, Vacuum, and Float Switches

Environment:
Pressure Switches Class 9013 FSG

Resolution:
Only if pressure release valve (form X) is not needed and the pressure range is suitable.